NXOpen.UF.Gexp.AskAngleParms¶
-
Gexp.
AskAngleParms
()¶ Refer to UF_GEXP_ask_angle_parms for documentation.
Signature:
AskAngleParms(featureTag)
Parameters: featureTag (Tag) – Tag of angle expression feature to query. Returns: A Tuple Return type: A tuple consisting of (object1,qualifier1,xform1,object2,qualifier2,xform2) object1(Tag): Tag of referenced object 1 the angle was created from
qualifier1(
`NXOpen.UF.Gexp.Qualifier
Refer to UF_GEXP_qualifier_e for documentation.`): Qualifier for object1, only applicable to lines and edges.xform1(Tag): Tag of transformation for first object; if the object is in the same part the feature was created in, this would be NULL_TAG.
object2(Tag): Tag of referenced object 2 the angle was created from.
qualifier2(
`NXOpen.UF.Gexp.Qualifier
Refer to UF_GEXP_qualifier_e for documentation.`): Qualifier for object2, only applicable to lines and edges.xform2(Tag): Tag of transformation for second object. This tag is NULL_TAG if the object is in the same part in which the feature was created.
License requirements: None