NXOpen.UF.Gdt.TargetRectArea Structure¶
NXOpen.UF.Gdt.TargetRectArea is an alias for NXOpen.UF.GdtTargetRectArea_Struct
-
class
NXOpen.UF.
GdtTargetRectArea_Struct
¶ Bases:
object
Refer to UF_GDT_target_rect_area_s for documentation.
Fields
NXOpen.UF.GdtTargetRectArea_Struct.DatumFeature |
This corresponds to the tag of the parent datum feature the target is to be applied to. |
NXOpen.UF.GdtTargetRectArea_Struct.TargetIndex |
Datum target index to assign to new datum targets. |
NXOpen.UF.GdtTargetRectArea_Struct.Point |
Identifier of smart point locating the center * of the target. |
NXOpen.UF.GdtTargetRectArea_Struct.IsPlanar |
Is this a planar datum target area? * Creation and Query routines only. |
NXOpen.UF.GdtTargetRectArea_Struct.Orientation |
Orientation of area relative to surface. |
NXOpen.UF.GdtTargetRectArea_Struct.Length |
Length of rectangular area |
NXOpen.UF.GdtTargetRectArea_Struct.Height |
Height of rectangular area |
NXOpen.UF.GdtTargetRectArea_Struct.Location |
Absolute position of target (output only) |