NXOpen.UF.Gdt.TargetDiaArea Structure¶
NXOpen.UF.Gdt.TargetDiaArea is an alias for NXOpen.UF.GdtTargetDiaArea_Struct
-
class
NXOpen.UF.
GdtTargetDiaArea_Struct
¶ Bases:
object
Refer to UF_GDT_target_dia_area_s for documentation.
Fields
NXOpen.UF.GdtTargetDiaArea_Struct.DatumFeature |
The tag of the parent datum feature the target is to be applied to. |
NXOpen.UF.GdtTargetDiaArea_Struct.TargetIndex |
Datum target index to assign to new datum targets. |
NXOpen.UF.GdtTargetDiaArea_Struct.Point |
Identifier of smart point locating the center * of the target. |
NXOpen.UF.GdtTargetDiaArea_Struct.Diameter |
Size of the outer datum target area diameter |
NXOpen.UF.GdtTargetDiaArea_Struct.InnerDia |
Size of the inner diameter for annular areas |
NXOpen.UF.GdtTargetDiaArea_Struct.IsPlanar |
Is this a planar datum target area? * Creation and Query routines only. |
NXOpen.UF.GdtTargetDiaArea_Struct.Orientation |
Orientation of area relative to surface. |
NXOpen.UF.GdtTargetDiaArea_Struct.Location |
Absolute position of target (output only) |