NXOpen.UF.GdtLeaderSpec_Struct.View |
Tag of view the leader terminates in |
NXOpen.UF.GdtLeaderSpec_Struct.Terminator |
Tag of object leader is attached to |
NXOpen.UF.GdtLeaderSpec_Struct.AttachPoint |
Point of the leader’s terminator |
NXOpen.UF.GdtLeaderSpec_Struct.StubPoints |
Stub start and end points. |
NXOpen.UF.GdtLeaderSpec_Struct.NumIntermediates |
Number of intermediate points |
NXOpen.UF.GdtLeaderSpec_Struct.Intermediates |
Array of intermediate leader points. |
NXOpen.UF.GdtLeaderSpec_Struct.Type |
The type of leader’s arrowhead |
NXOpen.UF.GdtLeaderSpec_Struct.IsProfileLeader |
Is the leader a profile leader |
NXOpen.UF.GdtLeaderSpec_Struct.Filled |
Is the leader’s arrowhead filled? |
NXOpen.UF.GdtLeaderSpec_Struct.AllAround |
Is the leader an all_around leader? |
NXOpen.UF.GdtLeaderSpec_Struct.AllAroundDiameter |
Diameter of the all around symbol |
NXOpen.UF.GdtLeaderSpec_Struct.DotDiameter |
Diameter of dot, if a dot terminator |
NXOpen.UF.GdtLeaderSpec_Struct.ArrowheadLength |
Length of the leader arrowhead |
NXOpen.UF.GdtLeaderSpec_Struct.ArrowheadAngle |
Angle of leader arrowhead (Degrees) |
NXOpen.UF.GdtLeaderSpec_Struct.StubLength |
Length of the leader’s stub |
NXOpen.UF.GdtLeaderSpec_Struct.Direction |
Direction of the leader’s stub |
NXOpen.UF.GdtLeaderSpec_Struct.ProfileTerm2 |
2nd profile leader attachment object |
NXOpen.UF.GdtLeaderSpec_Struct.ProfileAttach |
2nd profile leader attachment point |
NXOpen.UF.GdtLeaderSpec_Struct.ProfileLdrLength |
Length of the 2nd profile leader |
NXOpen.UF.GdtLeaderSpec_Struct.LeaderColor |
Color of the leader |
NXOpen.UF.GdtLeaderSpec_Struct.LeaderFont |
Font of the leader |
NXOpen.UF.GdtLeaderSpec_Struct.LeaderWidth |
(Line) Width of the leader * This width should be described * using the UF_OBJ_WIDTH definitions * in uf_obj.h |
NXOpen.UF.GdtLeaderSpec_Struct.ArrowheadColor |
Color of the leader’s arrowhead |
NXOpen.UF.GdtLeaderSpec_Struct.ArrowheadFont |
Font of the leader’s arrowhead |
NXOpen.UF.GdtLeaderSpec_Struct.ArrowheadWidth |
(Line) Width of leader’s arrowhead * This width should be described * using the UF_OBJ_WIDTH definitions * in uf_obj.h |
NXOpen.UF.GdtLeaderSpec_Struct.ArrowInfo |
Structure about the terminator. |