NXOpen.UF.Gdt.DatumTargetPoint Structure¶
NXOpen.UF.Gdt.DatumTargetPoint is an alias for NXOpen.UF.GdtDatumTargetPoint_Struct
-
class
NXOpen.UF.
GdtDatumTargetPoint_Struct
¶ Bases:
object
Refer to UF_GDT_datum_target_point_s for documentation.
Fields
NXOpen.UF.GdtDatumTargetPoint_Struct.PointOnSurface |
The identifier of the point which defines the target point |
NXOpen.UF.GdtDatumTargetPoint_Struct.PointData |
The actual position of the target on their referencing plane |
NXOpen.UF.GdtDatumTargetPoint_Struct.DatumFeature |
The identifier of the datum feature that the target constrains |
NXOpen.UF.GdtDatumTargetPoint_Struct.TargetIndex |
The identifier of the target point |