NXOpen.UF.Gdt.SetRegionParameters¶
-
Gdt.
SetRegionParameters
()¶ Refer to UF_GDT_set_region_parameters for documentation.
Signature:
SetRegionParameters(regionThickness, crosshatchOn, crosshatchAngle, crosshatchDistance)
Parameters: - regionThickness (float) – The region thickness which is to be used when regions for GDTs are created
- crosshatchOn (bool) – TRUE if the region of a GDT is to be crosshatched.
- crosshatchAngle (float) – The angle to be used when crosshatching a region
- crosshatchDistance (float) – The distance between hatch lines to be used when crosshatching a region
License requirements: GDT