NXOpen.UF.FbmGeom.AskIntValueOfClassifiedCrit¶
-
FbmGeom.
AskIntValueOfClassifiedCrit
()¶ Refer to UF_FBM_GEOM_ask_int_value_of_classified_crit for documentation.
Signature:
AskIntValueOfClassifiedCrit(fbmGeomTag, criterion, classifiedSetList, classifiedSetIndex)
Parameters: - fbmGeomTag (Tag) – The tag of the fbm_geom group of interest
- criterion (str) – The criteria for which the value is asked for
- classifiedSetList (PointerWrapper) – The result of the classification
- classifiedSetIndex (int) – The index of the set which should be used
Returns: The value of the criterion
Return type: int
License requirements: None