NXOpen.UF.Fam.FamilyData Structure¶
NXOpen.UF.Fam.FamilyData is an alias for NXOpen.UF.FamFamilyData_Struct
-
class
NXOpen.UF.
FamFamilyData_Struct
¶ Bases:
object
Refer to UF_FAM_family_data_s for documentation.
Fields
NXOpen.UF.FamFamilyData_Struct.Subtype |
A flag indicating which type of family this is. |
NXOpen.UF.FamFamilyData_Struct.AttributeCount |
The number of attributes of the family. |
NXOpen.UF.FamFamilyData_Struct.MemberCount |
The number of members in the family. |
NXOpen.UF.FamFamilyData_Struct.Attributes |
An array of family attribute tags which describe the parameters of the family. |
NXOpen.UF.FamFamilyData_Struct.Name |
The name for the family. |