NXOpen.UF.Fam.ClassData Structure¶
NXOpen.UF.Fam.ClassData is an alias for NXOpen.UF.FamClassData_Struct
-
class
NXOpen.UF.
FamClassData_Struct
¶ Bases:
object
Refer to UF_FAM_class_data_s for documentation.
Fields
NXOpen.UF.FamClassData_Struct.Subtype |
A flag indicating the type of attributes in this class. |
NXOpen.UF.FamClassData_Struct.AttributeCount |
The number of attributes in this class |
NXOpen.UF.FamClassData_Struct.AttributeData |
An array of family attribute structures(see below). |
NXOpen.UF.FamClassData_Struct.Name |
The name of the attribute class. |