NXOpen.UF.Facet.FacetSolid¶
-
Facet.
FacetSolid
()¶ Refer to UF_FACET_facet_solid for documentation.
Signature:
FacetSolid(solidEntity, parameters)
Parameters: - solidEntity (Tag) – The solid to be faceted
- parameters (
NXOpen.UF.Facet.Parameters
Refer to UF_FACET_parameters_s for documentation.) – The parameters to be used to facet the solid. If NULL is specified then the defaults are used.
Returns: The faceted model produced
Return type: License requirements: ASSEMBLIES MODULE