NXOpen.UF.Facet.CycleFacetsInFace¶
-
Facet.
CycleFacetsInFace
()¶ Refer to UF_FACET_cycle_facets_in_face for documentation.
Signature:
CycleFacetsInFace(model, faceId, facetId)
Parameters: - model (Tag) – The model.
- faceId (int) – The face whose facets are to be cycled.
- facetId (int) – On input the id of the current facet in the model. Pass in UF_FACET_NULL_FACET_ID to start the cycle. On output the id of the next facet in the model, if there are no more facets, UF_FACET_NULL_FACET_ID is returned.
Returns: Modified value of facetId
Return type: int
License requirements: ASSEMBLIES MODULE