NXOpen.UF.Facet.CycleFacets¶
-
Facet.
CycleFacets
()¶ Refer to UF_FACET_cycle_facets for documentation.
Signature:
CycleFacets(model, facetId)
Parameters: - model (Tag) – The faceted model to be cycled.
- facetId (int) – On input the id of the current facet in the model. Pass in UF_FACET_NULL_FACET_ID to start the cycle. On output the id of the next facet in the model, if there are no more facets, UF_FACET_NULL_FACET_ID is returned.
Returns: Modified value of facetId
Return type: int
License requirements: ASSEMBLIES MODULE