NXOpen.UF.Facet.AskAdjacentFacet¶
-
Facet.
AskAdjacentFacet
()¶ Refer to UF_FACET_ask_adjacent_facet for documentation.
Signature:
AskAdjacentFacet(model, facetId, edgeId)
Parameters: - model (Tag) – The model
- facetId (int) – The id of the facet.
- edgeId (int) – The edge of which the adjacent facet is being inquired.
Returns: A Tuple
Return type: A tuple consisting of (adjacentFacetId,edgeIdInAdjacentFacet)
adjacentFacetId(int): The adjacent facet
edgeIdInAdjacentFacet(int): The edge in the adjacent facet which is adjacent to edge_id in facet_id.
License requirements: None