NXOpen.UF.Eval.Ellipse Structure¶
NXOpen.UF.Eval.Ellipse is an alias for NXOpen.UF.EvalEllipse_Struct
-
class
NXOpen.UF.
EvalEllipse_Struct
¶ Bases:
object
Refer to UF_EVAL_ellipse_s for documentation.
Fields
NXOpen.UF.EvalEllipse_Struct.IsPeriodic |
Is the curve periodic or not? |
NXOpen.UF.EvalEllipse_Struct.Limits |
Curve limits: [0] = min; [1] = max |
NXOpen.UF.EvalEllipse_Struct.Minor |
Minor radius |
NXOpen.UF.EvalEllipse_Struct.Major |
Major radius |
NXOpen.UF.EvalEllipse_Struct.Center |
|
NXOpen.UF.EvalEllipse_Struct.XAxis |
Unit direction vector of the x axis (ABS) |
NXOpen.UF.EvalEllipse_Struct.YAxis |
Unit direction vector of the y axis (ABS) |