NXOpen.UF.Drf.UnitsFormatPreferences Structure¶
NXOpen.UF.Drf.UnitsFormatPreferences is an alias for NXOpen.UF.DrfUnitsFormatPreferences_Struct
-
class
NXOpen.UF.
DrfUnitsFormatPreferences_Struct
¶ Bases:
object
Refer to UF_DRF_units_format_preferences_s for documentation.
Fields
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DimensionLinearUnits |
linear units for primary value |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.LinearFractionType |
primary format -decimal or fractional |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DecimalPointCharacter |
use period or comma for decimal point |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DisplayTrailingZeros |
if TRUE, display zeros trailing a significant digit for dimension value |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DimensionTolerancePlacement |
placement of tolerance text relative to dimension text |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DimensionAngularFormat |
use decimal ordegree [minute] [second] format for angular nominal format only |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DimAngularFormatTolerance |
use decimal ordegree [minute] [second] format for angular tolerance format only |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.AngularSuppressZeros |
suppress zero options display all zeros, or suppress leading zeros, or suppress any zeros, or suppress trailing zeros for angular dimension only |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DualDimensionFormat |
set no dual dimension or specify placement of dual dimension relative to primary dimension |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DualDimensionUnits |
linear units for secondary value |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DualFractionType |
secondary format - decimal or fractional |
NXOpen.UF.DrfUnitsFormatPreferences_Struct.DualConvertTolerance |
if TRUE, secondary tolerance value will be computed from primary tolerance value |