NXOpen.UF.DrfUdsSize_Struct.UdsSizeType¶
-
DrfUdsSize_Struct.
UdsSizeType
¶ If the uds type is set to UF_DRF_LENGTH_HEIGHT, then the following * parameters are interpreted as ?length and height?. If the uds * type is set to UF_DRF_SCALE_ASPECT_RATIO, then the following * parameters are interpreted as ?scale and aspect ratio?.