NXOpen.UF.Drf.ToleranceType Enumeration¶
NXOpen.UF.Drf.ToleranceType is an alias for NXOpen.UF.DrfToleranceType
-
class
NXOpen.UF.
DrfToleranceType
¶ Bases:
object
Refer to UF_DRF_tolerance_type_e for documentation.
Enum Members
Enum Member NO_TOLERANCE LIMIT_ONE_LINE LIMIT_TWO_LINES BILATERAL_ONE_LINE BILATERAL_TWO_LINES UNILATERAL_ABOVE UNILATERAL_BELOW BASIC_TOL REFERENCE_TOL LIMIT_LARGER_FIRST LIMIT_LARGER_BELOW NOT_TO_SCALE_TOL DIAMETER_REFERENCE_TOL LIMIT_AND_FIT BASIC_DIM_NOT_TO_SCALE_TOL MAX_NUM_TOL