NXOpen.UF.DrfLeaderInfo_Struct.LeaderAttachType¶
-
DrfLeaderInfo_Struct.
LeaderAttachType
¶ Each leader may have up to 7 intermediate points. This is an array of the attachment types for each of the points. [0] is the information for the first point, [1] is for the second point, etc. Each element can have one of the values: UF_DRF_leader_attach_object UF_DRF_leader_attach_screen UF_DRF_leader_attach_triangle Only a GD&T symbol may have the type, UF_DRF_leader_attach_triangle.