NXOpen.UF.Drf.GdtLeaderData Structure¶
NXOpen.UF.Drf.GdtLeaderData is an alias for NXOpen.UF.DrfGdtLeaderData_Struct
-
class
NXOpen.UF.
DrfGdtLeaderData_Struct
¶ Bases:
object
Refer to UF_DRF_gdt_leader_data_s for documentation.
Fields
NXOpen.UF.DrfGdtLeaderData_Struct.Object |
This is the tag of the associated object. |
NXOpen.UF.DrfGdtLeaderData_Struct.View |
This is the tag of the member view of the object_tag entity. |
NXOpen.UF.DrfGdtLeaderData_Struct.Point |
This 3D point is the location of the terminator (or arrow) of the leader. |
NXOpen.UF.DrfGdtLeaderData_Struct.IntermediatePoints |
These are the intermediate points, if any, between the stub and the terminator of the leader. |