NXOpen.UF.DrfDiameterRadiusPreferences_Struct.TextAboveLeader¶
-
DrfDiameterRadiusPreferences_Struct.
TextAboveLeader
¶ if option is set to anything other than UF_DRF_NO_TEXT_ABOVE_LEADER, then dimension text will be displayed above the leader stub with the stub extended to the maximum length of the dimension text. used with dimension text orientations of UF_DRF_TEXT_DIMENSION_HORIZONTAL and UF_DRF_TEXT_DIMENSION_BY_ANGLE. for UF_DRF_NO_TEXT_ABOVE_LEADER, the di mension text displays next to the leader stub