NXOpen.UF.Drf.CustomSymbol Structure¶
NXOpen.UF.Drf.CustomSymbol is an alias for NXOpen.UF.DrfCustomSymbol_Struct
-
class
NXOpen.UF.
DrfCustomSymbol_Struct
¶ Bases:
object
Refer to UF_DRF_custom_symbol_s for documentation.
Fields
NXOpen.UF.DrfCustomSymbol_Struct.Geometry |
Tags of lines, arcs, splines, crosshatch, and area fill for symbol definition |
NXOpen.UF.DrfCustomSymbol_Struct.NumGeometry |
Number of tags in the curves array above. |
NXOpen.UF.DrfCustomSymbol_Struct.Text |
Array of symbol text structures for symbol definition. |
NXOpen.UF.DrfCustomSymbol_Struct.NumText |
Number of text structures in the text array. |
NXOpen.UF.DrfCustomSymbol_Struct.AnchorPoint |
Tag of the symbol’s anchor point. |
NXOpen.UF.DrfCustomSymbol_Struct.Connections |
Array of tags for the symbol’s leader connect points. |
NXOpen.UF.DrfCustomSymbol_Struct.NumConnections |
Number of leader connection points. |
NXOpen.UF.DrfCustomSymbol_Struct.Leader |
Pointer to information about the leader |
NXOpen.UF.DrfCustomSymbol_Struct.Angle |
The angle of the symbol with respect to the WCS X-axis |
NXOpen.UF.DrfCustomSymbol_Struct.Scale |
The scale of the symbol with respect to the size of the original geometry |
NXOpen.UF.DrfCustomSymbol_Struct.Origin |
The origin of the symbol in absolute coordinates. |