NXOpen.UF.Drf.CustomSymbolText Structure¶
NXOpen.UF.Drf.CustomSymbolText is an alias for NXOpen.UF.DrfCustomSymbolText_Struct
-
class
NXOpen.UF.
DrfCustomSymbolText_Struct
¶ Bases:
object
Refer to UF_DRF_custom_symbol_text_s for documentation.
Fields
NXOpen.UF.DrfCustomSymbolText_Struct.NoteTag |
This is the tag of the note from which this text will be based. |
NXOpen.UF.DrfCustomSymbolText_Struct.TextType |
The type of text for this structure |
NXOpen.UF.DrfCustomSymbolText_Struct.Title |
The title of this text field. |
NXOpen.UF.DrfCustomSymbolText_Struct.MinValue |
This value is the lower bound for UF_DRF_integer_text and UF_DRF_real_text types. |
NXOpen.UF.DrfCustomSymbolText_Struct.MaxValue |
This value is the upper bound for UF_DRF_integer_text and UF_DRF_real_text types. |
NXOpen.UF.DrfCustomSymbolText_Struct.CurrentValue |
This value is the current value defined for this text object. |
NXOpen.UF.DrfCustomSymbolText_Struct.OptionalStrings |
An array of strings in localized format describing a list of strings for controlled and partially controlled text. |
NXOpen.UF.DrfCustomSymbolText_Struct.NumOptionalStrings |
The number of strings in the array above. |
NXOpen.UF.DrfCustomSymbolText_Struct.CurrentOption |
The index of the currently selected string for controlled and partialy controlled text. |
NXOpen.UF.DrfCustomSymbolText_Struct.SimpleText |
The current value for arbitrary or mandatory text. |