NXOpen.UF.DrfAssociativeOrigin_Struct.OriginType |
Used for UF_DRF_ORIGIN_RELATIVE_TO_VIEW |
NXOpen.UF.DrfAssociativeOrigin_Struct.ViewEid |
View of associativity for the annotation. |
NXOpen.UF.DrfAssociativeOrigin_Struct.ViewOfGeometry |
The member view in which the absolute model * point lies. |
NXOpen.UF.DrfAssociativeOrigin_Struct.PointOnGeometry |
Absolute point in absolute space the annotation * is associated with. |
NXOpen.UF.DrfAssociativeOrigin_Struct.VertAnnotation |
Annotation to align * with. |
NXOpen.UF.DrfAssociativeOrigin_Struct.VertAlignmentPosition |
Alignment position on * vert_annotation to * align to. |
NXOpen.UF.DrfAssociativeOrigin_Struct.HorizAnnotation |
Annotation to align * with. |
NXOpen.UF.DrfAssociativeOrigin_Struct.HorizAlignmentPosition |
Alignment position on * horiz_annotation to * align to. |
NXOpen.UF.DrfAssociativeOrigin_Struct.AlignedAnnotation |
Alignment annotation |
NXOpen.UF.DrfAssociativeOrigin_Struct.DimensionLine |
1 for dimension line 1, 2 for dimension line 2 |
NXOpen.UF.DrfAssociativeOrigin_Struct.AssociatedView |
The member view in which the absolute model * point lies. |
NXOpen.UF.DrfAssociativeOrigin_Struct.AssociatedPoint |
Origin location of annotation |
NXOpen.UF.DrfAssociativeOrigin_Struct.OffsetAnnotation |
Annotation to align * to |
NXOpen.UF.DrfAssociativeOrigin_Struct.OffsetAlignmentPosition |
Alignment position * on annotation to * align with. |
NXOpen.UF.DrfAssociativeOrigin_Struct.XOffsetFactor |
X Offset factor from * associated point. |
NXOpen.UF.DrfAssociativeOrigin_Struct.YOffsetFactor |
Y Offset factor from * associated point. |
NXOpen.UF.DrfAssociativeOrigin_Struct.StackAnnotation |
Used for UF_DRF_ORIGIN_STACK |
NXOpen.UF.DrfAssociativeOrigin_Struct.StackAlignmentPosition |
|