NXOpen.UF.Drf.SetVerticalNote¶
-
Drf.
SetVerticalNote
()¶ Refer to UF_DRF_set_vertical_note for documentation.
Signature:
SetVerticalNote(note, isVertical)
Parameters: - note (Tag) – Tag of the note.
- isVertical (bool) – If TRUE, set the note to be vertical, if FALSE set the note horizontal. If the object is not a note, no action is taken, and the return code will be zero.
License requirements: DRAFTING