NXOpen.UF.Drf.SetAnnotationTemplate¶
-
Drf.
SetAnnotationTemplate
()¶ Refer to UF_DRF_set_annotation_template for documentation.
Signature:
SetAnnotationTemplate(annotationTemplateName)
Parameters: annotationTemplateName (str) – the name of the annotationtemplate part which will be used by UF_DRF_inherit_feature_data. The name is the same as the name appearing in the Feature Parameters dialog and does not contain the directory in which the part resides or the extension .atp.prt, for example, ansi or iso_din License requirements: DRAFTING