NXOpen.UF.Drf.InheritFeatureData¶
-
Drf.
InheritFeatureData
()¶ Refer to UF_DRF_inherit_feature_data for documentation.
Signature:
InheritFeatureData(featurePreV13SketchCount, featuresPreV13Sketches, partOccs, viewCount, views, inheritType)
Parameters: - featurePreV13SketchCount (int) – number of features and pre-v13 sketches to be annotated
- featuresPreV13Sketches (list of Tag) – feature_pre_v13_sketch_count the features and pre-v13 sketches to be annotated. A pre-v13 sketch tag is the tag in the part of the sketch, not in the part occurrence of the sketch.
- partOccs (list of Tag) – feature_pre_v13_sketch_count the i-th feature or sketch to be annotated occurs in the occurence of the part given by part_occs[i]. NULL_TAG is valid.
- viewCount (int) – number of views to be annotated
- views (list of Tag) – views to be annotated
- inheritType (
NXOpen.UF.Drf.InheritType
Refer to UF_DRF_inherit_type_e for documentation.) – the types of annotation to be inherited Currently only UF_DRF_inherit_feature_parameters is supported
License requirements: DRAFTING