NXOpen.UF.Drf.GetXhatchParms¶
-
Drf.
GetXhatchParms
()¶ Refer to UF_DRF_get_xhatch_parms for documentation.
Signature:
GetXhatchParms(xhatEid)
Parameters: xhatEid (Tag) – Object identifier of the desired crosshatch Returns: A Tuple Return type: A tuple consisting of (matName,intParms,realParms,rtc) matName(list of str): Material name of the crosshatch
intParms(list of int): Integer parameters of the crosshatch. This an array of nine elements (int_parms[9]) [0] = entity site [1] = line density [2] = filled arrowhead control [3] = crosshatch symbol color [4] = section validity flag [5-8] = number of crosshatch lines in each of 4 directions
realParms(list of float): Real parameters of the crosshatch. This is an array of 13 elements (real_parms[13]). [0] = Arrow size [1-4] = Crosshatch distance for each of 4 directions [5-8] = Crosshatch angle for each of 4 directions [9] = Crosshatch tolerance [10] = Arrowhead filled distance [11] = Arrowhead included angle [12] = Dot arrowhead diameter
rtc(int): Return code: 1 = xhat_eid is not a hatch.
License requirements: DRAFTING