NXOpen.UF.Drf.GetCharFont¶
-
Drf.
GetCharFont
()¶ Refer to UF_DRF_get_char_font for documentation.
Deprecated since version NX5.0.
Signature:
GetCharFont(fontIndex)
Parameters: fontIndex (int) – The font index number for which to get a font name. Currently, there are 14 possible character fonts. Returns: The font name at index number “findx”. The function outputs a C string. If there is no font at a particular index, the function outputs a blank string. Return type: list of str License requirements: DRAFTING