NXOpen.UF.Drf.Frdim¶
-
Drf.
Frdim
()¶ Refer to UF_DRF_frdim for documentation.
Signature:
Frdim(np1, np2, ip3, ip4, rp5, rp6, cp7, ip8, cp9, rp10)
Parameters: - np1 (Tag) – Object identifier of an Arc, bolt circle or circular CLINE.
- np2 (Tag) – Object identifier of offset center point (point, line, solid edge, offse center point, cylindrical center line, symmetrical center line, target point or intersection point.
- ip3 (int) – Type of associativity: 1 = endpoint 2 = Arc center 3 = Tangency
- ip4 (int) – Associativity modifier, if the type of associativity is an endpoint: 1 = Associate to first endpoint 2 = Associate to second endpoint If the type of associativity is a tangency: 0-100 is the parameter percent to be used to compute the approximate tangency point.
- rp5 (float) – Fold location in WCS coordinates.
- rp6 (float) – Fold angle in degrees.
- cp7 (str) – Dimension text string.
- ip8 (int) – Number of lines of appended text.
- cp9 (list of str) – Array of appended text strings.
- rp10 (list of float) – X, Y and Z of object origin in WCS coordinates.
Returns: A Tuple
Return type: A tuple consisting of (nr11,error)
nr11(Tag): Object identifier of the created folded radius dimension.
error(int): Error return, 0 for success.
License requirements: DRAFTING