NXOpen.UF.Drf.CreateOrdorigin¶
-
Drf.
CreateOrdorigin
()¶ Refer to UF_DRF_create_ordorigin for documentation.
Signature:
CreateOrdorigin(objectArg, positiveQuadId, arrDimLineDisplay, originSymbolDisplay, userObjectName)
Parameters: - objectArg (
NXOpen.UF.Drf.Object
Refer to UF_DRF_object_s for documentation.) – Data of object (see uf_drf_types.h) Valid object types: point, line, arc, conic, cubic spline, B curve, pattern, solid curve, offset center point, cylindrical, symmetrical centerline, intersection symbol, drafting point - positiveQuadId (int) – Positive quadrant identifier determines signs of dimensions 1 = upper right 2 = upper left 3 = lower right 4 = lower left 5 = all quadrants
- arrDimLineDisplay (int) – Arrow and dimension line display 1 = no 2 = yes
- originSymbolDisplay (int) – Origin symbol display 1 = origin name 2 = no display
- userObjectName (str) – User supplied object name
Returns: Object tag of created ordinate origin.
Return type: License requirements: DRAFTING
- objectArg (