NXOpen.UF.Drf.CreateOrdinateMargin¶
-
Drf.
CreateOrdinateMargin
()¶ Refer to UF_DRF_create_ordinate_margin for documentation.
Signature:
CreateOrdinateMargin(ip1, np2, np3, rp4, rp5, rp6)
Parameters: - ip1 (int) – Type of margin: 1 = Horizontal 2 = Vertical
- np2 (Tag) – Object identifier of the ordinate origin.
- np3 (Tag) – Object identifier of the line or a NULL_TAG.
- rp4 (list of float) – X, Y point on the margin, only used if no line object is passed in.
- rp5 (list of float) – X, Y direction of the margin, only used if no line object is passed in.
- rp6 (float) – Offset distance.
Returns: Object identifier of the created margin.
Return type: License requirements: DRAFTING