NXOpen.UF.Drf.CreateOrdinateDim¶
-
Drf.
CreateOrdinateDim
()¶ Refer to UF_DRF_create_ordinate_dim for documentation.
Signature:
CreateOrdinateDim(np1, ip2, np3, ip4, ip5, rp6, rp7, cp8, ip9, cp10, ip11, rp12)
Parameters: - np1 (Tag) – Object identifier of the margin or ordinate origin.
- ip2 (int) – Type of dimension if object is an origin: 1 = Horizontal 2 = Vertical
- np3 (Tag) – Object to be dimensioned.
- ip4 (int) – Type of associativity to the object 1 = Endpoint 2 = Arc center 3 = Tangency 4 = Utility symbol
- ip5 (int) – Associativity modifier. For endpoint associativity: 1 = First endpoint 2 = Second endpoint For a tangency associativity: 0-100 = parameter percent along the arc to identify the point used to pick the arc side to dimension. For a utility symbol: 1-100 centerline segment number
- rp6 (float) – Dogleg angle in degrees ( 0.0 for no dogleg).
- rp7 (float) – Dogleg distance from the dimension point in WCS units.
- cp8 (str) – Dimension text string.
- ip9 (int) – Number of lines of appended text.
- cp10 (list of str) – Array of appended text strings.
- ip11 (int) – Text origin flag: 1 = Center of total text box. 2 = Center of dimension text box
- rp12 (list of float) – X, Y and Z of origin in WCS coordinates.
Returns: Object identifier of created dimension
Return type: License requirements: DRAFTING