NXOpen.UF.Drf.CreateOrddimension¶
-
Drf.
CreateOrddimension
()¶ Refer to UF_DRF_create_orddimension for documentation.
Signature:
CreateOrddimension(marginOriginTag, dimensionType, objectArg, doglegAngle, doglegDistance, drfText, textOriginFlag, origin3d)
Parameters: - marginOriginTag (Tag) – Margin or origin tag
- dimensionType (int) – Type of dimension (required when margin_origin_tag is origin, ignored otherwise) 1 = horizontal 2 = vertical
- objectArg (
NXOpen.UF.Drf.Object
Refer to UF_DRF_object_s for documentation.) – Data of object (see uf_drf_types.h) valid object types: point, line, arc, conic, cubic spline, B curve, pattern, solid curve, offset center point, cylindrical, symmetrical centerline, intersection symbol, target point - doglegAngle (float) – Dogleg angle in degrees (0.0 for no dogleg)
- doglegDistance (float) – Dogleg distance from dim point in wcs coordinates
- drfText (
NXOpen.UF.Drf.Text
Refer to UF_DRF_text_s for documentation.) – Associated text (see uf_drf_types.h) - textOriginFlag (int) – Text origin flag 1 = center of total text box 2 = center of dimension text box
- origin3d (list of float) – 3d dimension origin in wcs coordinates
Returns: Object tag of created ordinate dimension.
Return type: License requirements: DRAFTING