NXOpen.UF.Drf.CreateNonAssocHatch¶
-
Drf.
CreateNonAssocHatch
()¶ Refer to UF_DRF_create_non_assoc_hatch for documentation.
Signature:
CreateNonAssocHatch(numLines, hatchLines, matrix, view, color, lineWidth)
Parameters: - numLines (int) – number of hatch lines = sizeof(hatch_lines)/4
- hatchLines (list of float) – num_linescrosshatch lines ([x1, y1, x2, y2]) quadruples As with all annotations the coordinates are in the coordinater system of the matrix
- matrix (Tag) – matrix for crosshatch if NULL_TAG then the matrix of the WCS is used
- view (Tag) – view of crosshatch if NULL_TAG then the crosshatch is not view dependent
- color (int) – color
- lineWidth (int) – line width
Returns: crosshatch created or NULL_TAG if error
Return type: License requirements: DRAFTING