NXOpen.UF.Drf.CreateLinearCline¶
-
Drf.
CreateLinearCline
()¶ Refer to UF_DRF_create_linear_cline for documentation.
Signature:
CreateLinearCline(numClineObjs, clineObjList)
Parameters: - numClineObjs (int) – Number of centerline objects in cline_obj_list Maximum is MAX_CENTERLINE_OBJECTS, currently 100
- clineObjList (list of
NXOpen.UF.Drf.Object
Refer to UF_DRF_object_s for documentation.) – Array of objects that are to be associated to the centerline (see uf_drf_types.h) Valid object types: point, arc, solid curve
Returns: Object tag of created centerline
Return type: License requirements: DRAFTING