NXOpen.UF.Drf.CreateImageFromFile¶
-
Drf.
CreateImageFromFile
()¶ Refer to UF_DRF_create_image_from_file for documentation.
Signature:
CreateImageFromFile(fileName, drawingSheet, origin)
Parameters: - fileName (str) – Name of jpg, png or tif file to use to create image
- drawingSheet (Tag) – The drawing sheet on which to create the image or NULL_TAG to create the image on the current drawing sheet.
- origin (list of float) – Origin of new image in drawing sheet units
Returns: Image tag if successful or NULL_TAG if creation failed
Return type: License requirements: DRAFTING