NXOpen.UF.Drf.CreateImage¶
-
Drf.
CreateImage
()¶ Refer to UF_DRF_create_image for documentation.
Signature:
CreateImage(imageName, drawingSheet, origin)
Parameters: - imageName (str) – Name of image in part file
- drawingSheet (Tag) – The drawing sheet on which to create the image or NULL_TAG to create the image on the current drawing sheet.
- origin (list of float) – Origin of new image in drawing sheet units
Returns: Image tag if successful or NULL_TAG if creation failed
Return type: License requirements: DRAFTING