NXOpen.UF.Drf.CreateCylindricalDim¶
-
Drf.
CreateCylindricalDim
()¶ Refer to UF_DRF_create_cylindrical_dim for documentation.
Signature:
CreateCylindricalDim(object1, object2, drfText, dimension3dOrigin)
Parameters: - object1 (
NXOpen.UF.Drf.Object
Refer to UF_DRF_object_s for documentation.) – Data of first object (see uf_drf_types.h) Valid object types: point, line, arc, conic, cubic spline, B curve, pattern, solid curve, utility symbol (centerline), or cylindrical face(if one associative object is a cylindrical face, both associative objects must be the same face. If the face is perpendicular to WCS X-Y plane the associative type must be tangency type). - object2 – Data of second object
- drfText (
NXOpen.UF.Drf.Text
Refer to UF_DRF_text_s for documentation.) – Associated text (see uf_drf_types.h) - dimension3dOrigin (list of float) – 3d dimension origin in wcs coordinates
Returns: Object tag of created cylindrical dimension
Return type: License requirements: DRAFTING
- object1 (