NXOpen.UF.Drf.CreateCptClineFbolt¶
-
Drf.
CreateCptClineFbolt
()¶ Refer to UF_DRF_create_cpt_cline_fbolt for documentation.
Signature:
CreateCptClineFbolt(numClineObjs, clineObjList, centerPoint)
Parameters: - numClineObjs (int) – Number of centerline objects in cline_obj_list Maximum is MAX_CENTERLINE_OBJECTS, currently 100
- clineObjList (list of
NXOpen.UF.Drf.Object
Refer to UF_DRF_object_s for documentation.) – Array of objects that are to be associated to the centerline (see uf_drf_types.h) - centerPoint – Data of object selected for centerline center point (see uf_drf_types.h)
Returns: Object tag of created centerline
Return type: License requirements: DRAFTING