NXOpen.UF.Drf.AskVerticalNote

Drf.AskVerticalNote()

Refer to UF_DRF_ask_vertical_note for documentation.

Signature: AskVerticalNote(note)

Parameters:note (Tag) – Tag of the note.
Returns:Orientation of the note: True if the note is vertical False if the note is horizontal If the object is not a note, False is returned.
Return type:bool

License requirements: None