NXOpen.UF.Drf.AskTextData¶
-
Drf.
AskTextData
()¶ Refer to UF_DRF_ask_text_data for documentation.
Signature:
AskTextData(ip1, annData)
Parameters: - ip1 (int) – Segment Number 1
- annData (list of int) – Array of ann_data returned by UF_DRF_ask_ann_data
Returns: A Tuple
Return type: A tuple consisting of (annData,cr3,ir4,ir5)
annData(list of int): Modified value of annData
cr3(str): Text String Must be freed by calling UF_free
ir4(int): Length of Line in 1/64th’s Character Size, Expressed in Integers
ir5(int): Number of Characters in String
License requirements: None