NXOpen.UF.Drf.AskPreferences¶
-
Drf.
AskPreferences
()¶ Refer to UF_DRF_ask_preferences for documentation.
Signature:
AskPreferences()
Returns: A Tuple Return type: A tuple consisting of (mpi,mpr,radiusValue,diameterValue) mpi(list of int): MPI Array [100 elements] The size of this array is defined by NUM_INT_PARAMS
mpr(list of float): MPR Array [70 elements] The size of this array is defined by NUM_REAL_PARAMS
radiusValue(list of str): Radius Symbol String. This can be at most six characters, however due to internal requirements, the buffer must be allocated as char radius_value[27];
diameterValue(list of str): Diameter Symbol String. This can be at most six characters, however due to internal requirements, the buffer must be allocated as char diameter_value[27];
License requirements: None