NXOpen.UF.Drf.AskObjectPreferences¶
-
Drf.
AskObjectPreferences
()¶ Refer to UF_DRF_ask_object_preferences for documentation.
Signature:
AskObjectPreferences(drfObjectTag)
Parameters: drfObjectTag (Tag) – Drafting object Identifier Returns: A Tuple Return type: A tuple consisting of (mpi,mpr,radiusVal,diameterVal) mpi(list of int): MPI Array [100 elements] The size of this array is defined by NUM_INT_PARAMS
mpr(list of float): MPR Array [70 elements] The size of this array is defined by NUM_REAL_PARAMS
radiusVal(list of str): Radius Symbol String. This can be at most six characters, however due to internal requirements, the buffer must be allocated as char radius_val[27];
diameterVal(list of str): Diameter Symbol String. This can be at most six characters, however due to internal requirements, the buffer must be allocated as char diameter_val[27];
License requirements: None