NXOpen.UF.Drf.AskDispParms¶
-
Drf.
AskDispParms
()¶ Refer to UF_DRF_ask_disp_parms for documentation.
Signature:
AskDispParms()
Returns: A Tuple Return type: A tuple consisting of (ir1,rr2) ir1(int): A 10 element array that will be filled with the drafting display parameters. The elements of the arrary are defined as: (0) MARGIN DISPLAY 1 = DISPLAY MARGINS 2 = DO NOT DISPLAY MARGINS (1) FAST FONT 1 = FAST FONT ON 2 = FAST FONT OFF (2) TEXT BOX MODE 1 = TEXT BOX MODE ON 2 = TEXT BOX MODE OFF (3) INDICATOR SITE 1 = DISPLAY INDICATOR SITE 2 = DO NOT DISPLAY INDICATOR SITE (4) TEXT SCALING FOR PART MERGE AND TRANSFORMATIONS 1 = SCALE TEXT 2 = DO NOT SCALE TEXT (5) FILLED ARROWHEAD DISPLAY 1 = DISPLAY FILLED ARROWHEAD 2 = DO NOT DISPLAY FILLED ARROWHEAD (6) - (9) RESERVED FOR FUTURE USE
rr2(float): A 5 element array that will be filled with the drafting display parameters. Currently only the first parameter rr2[0] is used. rr2[0] holds the character slant (in degrees).
License requirements: None