NXOpen.UF.Drf.AskArrowData¶
-
Drf.
AskArrowData
()¶ Refer to UF_DRF_ask_arrow_data for documentation.
Signature:
AskArrowData(dataBlock)
Parameters: dataBlock (list of int) – Only the following array elements are used: [0] = drafting object identifier [4] = record instance - If a label had 4 leaders, it would then have 4 arrows thus possible record instance values of 1, 2, 3 and 4. Returns: A Tuple Return type: A tuple consisting of (arrowType,filled,origin,arrowAngle,includeAngle,arrowHeight,arrowLength) arrowType(int): 1 = Closed Arrow 2 = Open Arrow 3 = Arch Cross 4 = Dot 5 = Origin symbol 6 = None
filled(int): The arrow head is either filled or open: 0 = open 1 = filled
origin(list of float): The x and y coordinates of the arrowhead: [0] = x-coordinate [1] = y-coordinat e
arrowAngle(float): The angle of the arrow line (degrees)
includeAngle(float): The arrowhead included angle (degrees)
arrowHeight(float): The height of the arrowhead. If the arrowhead type is 4 (dot), then this is the diameter of the dot.
arrowLength(float): The length of the arrowhead
License requirements: None