NXOpen.UF.Draw.ArrowParms Structure¶
NXOpen.UF.Draw.ArrowParms is an alias for NXOpen.UF.DrawArrowParms_Struct
-
class
NXOpen.UF.
DrawArrowParms_Struct
¶ Bases:
object
Refer to UF_DRAW_arrow_parms_s for documentation.
Fields
NXOpen.UF.DrawArrowParms_Struct.Size |
Arrow size must be greater than 0. |
NXOpen.UF.DrawArrowParms_Struct.TotalLength |
Arrow total length (must be greater than 0) @@ (B in the figure above) @@ |
NXOpen.UF.DrawArrowParms_Struct.InclAngle |
Arrow included angle (must be greater than 0) @@( C in the figure above ) @@ |
NXOpen.UF.DrawArrowParms_Struct.PastPartDist |
Arrow past part(must be greater than 0) @@ IMG=uf_draw_grf13.gif Figure Arrow Past Part Distance @@ |
NXOpen.UF.DrawArrowParms_Struct.StubLen |
Arrow stub length (must be greater than 0) @@ IMG=uf_draw_grf14.gif Figure Stub Length @@ |
NXOpen.UF.DrawArrowParms_Struct.HeadType |
Arrow head type UF_DRAW_ansi_arrow = ansi arrow UF_DRAW_iso_arrow = iso arrow @@ IMG=uf_draw_grf15.gif Figure Ansi vs. |
NXOpen.UF.DrawArrowParms_Struct.HeadControl |
Arrow head control (style) (must be greater than 0) UF_DRAW_open_arrowhead UF_DRAW_closed_arrowhead UF_DRAW_filled_arrowhead @@ IMG=uf_draw_grf16.gif Figure Arrowhead Style @@ |