NXOpen.UF.Draw.SetViewThdAppPitch¶
-
Draw.
SetViewThdAppPitch
()¶ Refer to UF_DRAW_set_view_thd_app_pitch for documentation.
Signature:
SetViewThdAppPitch(view, appPicth)
Parameters: - view (Tag) – tag of drawing member view
- appPicth (float) – This is a double value representing the new minimum apparent pitch for the view. This means that although a thread may have a smaller pitch, the smallest pitch which will be drawn is specified by app _pitch for visual clarity. For example, if a thread had a pitch of 0.001 inches but the minimum apparent pitch was 0.1, the thread would be drawn showing a pitch of 0.1, although the actual modelling data remains unchanged with a true pitch of 0.001 inches. the minimum apparent pitch for the view
License requirements: DRAFTING