NXOpen.UF.Draw.RedefineSxlineHinge¶
-
Draw.
RedefineSxlineHinge
()¶ Refer to UF_DRAW_redefine_sxline_hinge for documentation.
Signature:
RedefineSxlineHinge(sxlineTag, hingeLine, arrowSameDir)
Parameters: - sxlineTag (Tag) – section line tag
- hingeLine (
NXOpen.UF.Drf.LineObject
Refer to UF_DRF_line_object_s for documentation.) – object to associate hinge line to - arrowSameDir (bool) – If true, the new arrow direction will point away from the new hinge line in the same relative direction as the old arrow pointed away from the old hinge line. Else, the direction is flipped.
License requirements: DRAFTING