NXOpen.UF.Draw.EditBoundaryPoint¶
-
Draw.
EditBoundaryPoint
()¶ Refer to UF_DRAW_edit_boundary_point for documentation.
Signature:
EditBoundaryPoint(definingPoint, newPoint, viewTag)
Parameters: - definingPoint (Tag) – Tag of the defining point which is to be replaced
- newPoint (Tag) – Tag of the new point which will replace the defining point.
- viewTag (Tag) – Tag of the view whose defining point is being replaced. The view must have a break line/detail type boundary, and the boundary must be associated to model geometry (via UF_DRAW_set_boundary_assoc).
License requirements: DRAFTING