NXOpen.UF.Draw.AskSxsolidsOfSxview¶
-
Draw.
AskSxsolidsOfSxview
()¶ Refer to UF_DRAW_ask_sxsolids_of_sxview for documentation.
Signature:
AskSxsolidsOfSxview(sxviewTag, legNum)
Parameters: - sxviewTag (Tag) – Tag of section view
- legNum (
NXOpen.UF.Draw.SxlineLeg
Refer to UF_DRAW_sxline_leg_e for documentation.) – Leg number of the cut, UF_DRAW_sxline_leg1 or UF_DRAW_sxline_leg2. Required only if sxview_tag was created from a two legged revolved section line.
Returns: A Tuple
Return type: A tuple consisting of (numSxsolids,sxsolidTags)
numSxsolids(int): Number of solid sections created by the sectioning of the input leg.
sxsolidTags(list of Tag): Array of solid sections created by the sectioning of the input leg. Use UF_free to free memory.
License requirements: None